Monocyte removal for the fractionation of lymphocytes from PBMCs
CELLNETTA Application Case Studies
There is extensive research being conducted on regenerative medicine products that use human blood and tissue as raw materials for drugs.
The specific cells used as these raw materials for drugs should not be contaminated with other cells. Therefore, a highly accurate method is required to extract the desired cells from the original blood or tissue.
Magnetic beadseparation is used as a method for separating cells, but the reaction between cells and antibodies, as well as the process ofwashing the antibodies after separation, makes it a time-consuming process.
Therefore, we propose CELLNETTA, which can help speed up the process. Cells of different sizes can be easily sorted by simply pouring the cell suspension through CELLNETTA.
Here, we will introduce a case study on the use of CELLNETTA for the removal of monocytes for the fractionation of lymphocytes from human PBMCs (peripheral blood mononuclear cells), conducted by Dr. Norihisa Mikami of the Research and Development Department of RegCellCo., Ltd. (As of October 2021)
(Also available as a video)
Implementation method
- (1)Use buffer*1 to adjust the cell count of the human PBMCs to 5×106 cells/mL.
- (2)Apply hydrophilic treatment to the CELLNETTA.*2
- (3)Pour 1 ml of the cell suspension prepared in (1) through CELLNETTA.
- (4)Ensure that the fluid flows through, then pour 5 mL of buffer.
- (5)Use magnetic beads to further purify the cell suspension that has flowed through CELLNETTA, then analyze using flow cytometry*3.
*1 How to prepare the buffer (for 500 ml sample)
| D-PBS | 489 mL |
|---|---|
| FBS | 10 mL (final concentration of 2 %) |
| 0.5 mol/L EDTA solution | 1 mL (final concentration of 1 mM) |
*2 For more information, please refer to the “Hydrophilic Treatment Manual“ in the CELLNETTA User Guide.
*3 For magnetic bead purification and flow cytometry procedures, please refer to the manufacturer's operating procedures.
Results
Human PBMCs contain a large number of lymphocytes and monocytes.
Because lymphocytes have a smaller cell size than monocytes, CELLNETTA was used in an attempt tosort them by size.
Processing human PBMCs using a 7 µm mesh CELLNETTA showed a decrease in monocytes in the flow-through fraction (Figure 1).
Next, in order to adapt to the preparation of T cells to be used as raw materials for regenerative medicine products, CD4-positive T cells were purified with magnetic beads after monocyte removal using CELLNETTA or anti-CD14 antibody labeled magnetic beads.
As a result, both CELLNETTA and CD14 negative selection suppressed the monocyte contamination observed in untreated human PBMCs after CD4 purification (Figure 2).
These results indicate that CELLNETTA can be used to remove monocytes and to fractionate lymphocytes from human PBMCs.
The simple and quick operation of pouring human PBMCs through CELLNETTA can save time when compared to conventional methods.
For this reason, it is expected to contribute to reducing the manufacturing costs of regenerative medicine products.
Results of flow cytometry analysis : use of CELLNETTA reduced the percentage of Monocytes.
Positive selection using CD4 antibodies
(A)
(B)
(C)
Results of magnetic bead purification and flow cytometry analysis of the number of CD4-positive cells: CD4-positive cells can be recovered using CELLNETTA or CD14 negative selection.
Product used in this application note
| Pore size | Gamma Irradiation | Package Quantity | Product number (P/N) |
|---|---|---|---|
| 7 µm (custom made) | Gamma Irradiated | 1 | MZM1B007B50G |
Notes
- ●This product is not a medical device.
- ●This product is a sample for evaluation purpose.
- ●Please do not ship out your completed product with the sample.
- ●We shall not be liable for any claims on the sample in case it is shipped out to the market.
CELLNETTA Details
For purchasing inquiries, click here. For product inquiries, click here.
This product is single-use only.
- Compatible with 50 mL centrifuge tubes
- Individually packaged
- Made in Japan
- Gamma irradiated
| Size compatible with 50 mL centrifuge tubes | |||
|---|---|---|---|
| Pore Size (μm) | Package Quantity | Part Number | Application Examples |
| 5 | 1 | MZM1B005B50GA | Purification of culture medium from cell suspensions Removal of red blood cells from whole blood/PBMC |
| 5 | MZM1B005B50GB | ||
| 10 | 1 | MZM1B010B50GA | Purification of single cells |
| 5 | MZM1B010B50GB | ||
| 15 | 1 | MZM1B015B50GA | Fractionation of clusters and single cells |
| 5 | MZM1B015B50GB | ||
| 20 | 1 | MZM1B020B50GA | Fractionation of clusters and single cells |
| 5 | MZM1B020B50GB | ||
| 100 | 1 | MZM1B100B75GA | Spheroid size-based sorting for drug efficacy testing |
| 5 | MZM1B100B75GB | ||
| 200 | 1 | MZM1B200B75GA | Fractionation of microcarrier beads Spheroid size control |
| 5 | MZM1B200B75GB | ||
*We recommend selecting a pore size slightly smaller than the target cells. Please contact us for guidance on selecting the optimal pore size for your application.
*Flow behavior may vary depending on cell morphology, flow conditions, and other factors.